版本协议

BSD

标签
标准版
#第一届立创大赛#无线数字对讲模块

创建时间:7年前

项目主题:IoT(物联网)

8930 9

描述

<p>U/V双频数字&模拟对讲模块  一、<strong><strong>作品简介</strong></strong> 1、功能简介: 这种小功率无线对讲模块可集成于各种设备中,亦可独立使用。数字制式通话时,只能相同协议的模块间通话,可实现一对一和一对多,可以收发数据或者文字消息。模拟制式兼容传统的调频对讲机。</p> <p><strong>2、原理简介:</strong> <strong>该模块采用STM32F103R8T6做为主控,通过SPI和I2C与SX1278通信,通过I2C与RDA1846S通信,通过SPI和I2C与WM8974通信。SX1278和RDA1846S共用发射接收电路,通过PE4259切换。发射使用了两级放大,预计可以推到5W功率输出。接收前级使用了2个独立的低噪管NE3509(噪声系数0.5),每个负责一个频段,后级使用了MGA-685T6 集成的宽带低噪放大芯片(噪声系数0.93)。接收总增益有40dB,但是考虑噪声影响,估计信号增益是30dB左右。</strong></p> <p><strong>电源部分使用了基于XL6007的自动升降压电路,以便使功放管能够有稳定的7.5V漏极偏置电压,这样输出比较稳定,5-10V输入电压都能正常工作。</strong> STM32主要运行Speex语音编解码算法,将语音压缩后的数据通过SPI接口传递给SX1278打包发射。对端接收后包数据后解压缩可以还原成语音。当只需要模拟对讲时,应关闭SX1278,单独控制RDA1846工作,两者不能同时用于通信。STM32通过SPI以及额外的时钟信号与WM8974双工通信,在数字对讲时,可以实现打手机一样边说边听。 天线端的线路切换使用了Pin二极管,因为大功率的多通道射频开关很贵。输入线路和输出线路均加有低通滤波网络,抑制谐波 。</p> <p>3、PCB<strong>简介:</strong> 整体采用4层板设计,板厚1.6mm,敷铜厚35um,三个FR-4隔层分别厚0.2mm、1.1mm、0.2mm。层叠顺序为信号-地-电源-信号,在介电常数4.3的情况下,顶层50Ω微带线宽度应为0.3mm,但功率走线可以设计宽些,我设为0.35mm。</p> <p>功率芯片下面大量做通孔,既可以加速散热又可以降低接地阻抗。绕线电感尽量远离,或垂直摆放,减少不需要的耦合。功率管的匹配应通过矢量网络分析仪和频谱分析仪现场调试,低噪声放大器的匹配用ADS软件仿真设计完成,中心频点分别为144MHz和430MHz。天线端的线路切换使用了Pin二极管,因为大功率的多通道射频开关很贵。接收线路尽量远离了功放,以降低热噪声,底层在功放的位置开有镀锡散热窗,应粘上散热片。</p> <p>二、<strong>作品亮点</strong> 1、采用扩频传输、设计了PA和LNA电路,使得通信距离较远; 2、双频段电路设计,使得频率选择范围宽广,不用担心频道被占用。低频段配长天线信号穿透性绕射性都更好; 3、留有USB接口和仿真器接口,串口、I2C、SPI接口引出,整体可以作为开发板,可自行升级固件或者编程开发; 4、板载自动升降压的SEPIC稳压电源,输入电压选择范围较宽; 5、外扩I2C接口设备,键盘、显示屏、蓝牙模块。</p> <p><strong>三、**</strong>系统构架图<strong>**</strong> <strong><img src="//image.lceda.cn/pullimage/BQRJ4MJSWMy8SmsPN35oJoBZfWBLpABOqD1Ya6MU.jpeg" alt="1.jpg"></strong> <strong>   <img src="//" alt=""></strong> 四、<strong><strong>原理图</strong></strong> 原理图中射频部分元件值仅供参考。 <img src="//image.lceda.cn/pullimage/sU6WNibcJiGh8zTxPqb1QTFLrrp5iKiiW1Ga54hD.jpeg" alt="1.jpg"> <strong><img src="//" alt=""></strong> <strong>五、**</strong>材料清单(<strong><strong>BOM</strong></strong>列表<strong>**)</strong> <img src="//image.lceda.cn/pullimage/yNROnHUHSqEjh4KvK52g0I84D7t8N3XEXnmwwCwY.jpeg" alt="5.jpg">       <img src="//" alt=""> <strong>六、**</strong>PCB<strong>**实物图</strong> <img src="//" alt=""><img src="//image.lceda.cn/pullimage/TUdDHDS6dwwUrGl9kOmvaf2rM9dPBXCLF6xFRoQZ.jpeg" alt="6.jpg"> <img src="//image.lceda.cn/pullimage/MHOkX8CUsN4kl8Z9Mn1eQCgzvLrpXAkvYg4AD0nc.jpeg" alt="7.jpg"></p> <p><img src="//" alt=""> <img src="//" alt=""><img src="//image.lceda.cn/pullimage/T4GMOKvJd41rvRY2PT5tQa2PiZXoZaSDl6NU7i9L.jpeg" alt="8.jpg"></p> <p><strong>七、软件部分的描述</strong>      The Speex codec is an open-source, patent- and royalty-free software dedicated to speech compression and decompression.      Speex is based on CELP (code-excited linear prediction) and designed to compress voice at bitrates ranging from 2 to 44 kbps.      The features of Speex include:      – Narrowband (8 kHz), wideband (16 kHz), and ultrawideband (32 kHz) compression in the same bitstream      – Intensity stereo encoding      – Packet loss concealment      – Variable bitrate operation (VBR)      – Voice activity detection (VAD)      – Discontinuous transmission (DTX)      – Fixed-point port      – Acoustic echo canceller      – Noise suppression     还是移步这里来看吧 <a href="http://www.stmcu.org/document/detail/index/id-200260%E6%88%96%E8%80%85http://www.docin.com/p-702959468.html" target="_blank">http://www.stmcu.org/document/detail/index/id-200260或者http://www.docin.com/p-702959468.html</a>     还有<a href="http://bbs.eeworld.com.cn/thread-341817-1-1.html" target="_blank">http://bbs.eeworld.com.cn/thread-341817-1-1.html</a><br> <br> <strong>八、调试过程</strong> <img src="//" alt=""><img src="//image.lceda.cn/pullimage/WxrW3nEmP5o0wEsDlgMjjuQGxSacVGGSss4isDhs.jpeg" alt="1.jpg"><img src="//" alt=""> <img src="//image.lceda.cn/pullimage/9lrkxEJiVZbVRHEyqzjrpbvz8xIv41pKDUa3WwPi.jpeg" alt="2.jpg"> 焊好主要元件后首先测试电压。回流焊后,QFN封装的元件容易短路和虚焊,解决办法就是用热风枪开到350度补焊,提起来再压压紧就可以了。密集的引脚如果有焊锡粘连,用烙铁头熬上松香或者焊锡膏再去刷几下,多出的焊锡就会被烙铁头吸走。烙铁应尽量避免敲击,会敲坏发热芯,使用高温棉去除焊锡。如果氧化了,可以用复活膏短时间修复一阵。  现在3.3V、5V、7.5V电压都OK了,静态电流40mA。但是用手指触摸偏置线圈后,前级PA和后级PA之间随即产生自激振荡,使得7.5V电流达到1.6A,非常危险。解决办法就是重新调整RQA004和RQA0011之间的匹配网络,使得RQA0004的输出阻抗和RQA0011的输入阻抗达成共轭匹配,消除信号反射。使用网分和延长线,把C25移开,分别对前测反射S参数和对后测反射S参数,如图所示,失配比较严重,转到ADS软件里用史密斯圆图工具完成前后级的匹配,应注意,因为网分输出功率只有10dBm,只能测试小信号阻抗,所以结果只能作参考。 偏置电阻重新调整了大小,保证功率管偏置电流在容许范围内,级间匹配参照datasheet和网分的测试结果重新调整,已经不振荡了。 射频功放匹配调试过程: 1)热机半小时,然后把网分做双端口校准,保存。然后在1端口接上开路延长线,网分里找到延长线补偿选项,调整补偿参数,使得S11各频点阻抗数值集中到史密斯圆图最右顶端,保存; 2)确认PA的偏置电压都能达到指定值后,从前级开始调。首先应保证RQA0004的输入反射小于-10dB。打开ADS导入RQA0004的S2P模型做仿真设计,然后将结果应用到板上,如果还有振荡,可以在PA的输入端并联 68欧电阻串220pF电容到地,可以吃掉大部份的低频信号,低频信号自激振荡的源头。在仿真的基础上稍微调整电感和电容值后,测试430MHz S11</p> <p><strong>更多项目详情见链接:</strong><a href="http://club.szlcsc.com/article/details_482_1.html" target="_blank">http://club.szlcsc.com/article/details_482_1.html</a> <strong>本项目归立创社区“</strong>生日的蛋糕<strong>”所有</strong></p>

文档

BOM

暂无

附件

暂无

评论(0)

  • 表情
    emoji
    小嘉工作篇
    小嘉日常篇
  • 图片
成功
工程所有者当前已关闭评论
goToTop
svg-battery svg-battery-wifi svg-books svg-more svg-paste svg-pencil svg-plant svg-ruler svg-share svg-user svg-logo-cn svg-double-arrow